3/26/2018 12:40 AM | |
Joined: 3/17/2018 Last visit: 9/16/2019 Posts: 2 Rating:
|
Hi, I have 1214C DC/DC/DC CPU which has two Analog input channels that accept 0-10V DC signal. I want to connect a loop powered transmitter that outputs 4-20 mA, to the AI channel. Is it possible with the help of resistances? If so, please provide the wiring diagram. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/26/2018 10:15:29 AMNew subject after splitting |
|
3/26/2018 1:54 AM | |
Joined: 9/27/2006 Last visit: 3/6/2021 Posts: 10472 Rating:
|
Hello tvr; See if the answers here can provide the answers you seek: https://support.industry.siemens.com/tf/ww/en/posts/0-10-v-to-4-20-ma/142267?page=0&pageSize=10 hope this helps, |
3/28/2018 4:44 PM | |
Joined: 5/8/2016 Last visit: 2/2/2021 Posts: 167 Rating:
|
using norm and scale function in the program to adjust the span and zero accoring to your selection to the resistance kindly find the wiring diagram in the image attached regards, if that helpful please rate ahmed hamad
|
A lot of potential remains |
|
12/11/2018 6:04 PM | |
Joined: 12/11/2018 Last visit: 6/1/2019 Posts: 1 Rating:
|
Hi Thanks for the drawing, it really helped
|
Follow us on