1/17/2012 2:28 PM | |
Joined: 4/24/2006 Last visit: 9/23/2024 Posts: 8742 Rating: (1168) |
Hello, Have you seen this faq: how do you perform non-volatile saving of changed parameter data as variable ranges in the CPU's internal EEPROM memory? Best regards, Wizard |
1/18/2012 9:30 AM | |
Posts: 31 Rating: (0) |
Thx,i didnt konow there is possibility to indirectly write data to eeprom(didn find in manual S7-200 Programmable Controller System Manual).. please check out this peace of code.I thing it should work,not tested yet. THX for your reply,very useful Attachmentwriting to eeprom.zip (183 Downloads) |
1/24/2012 10:23 AM | |
Posts: 31 Rating: (0) |
Any suggestion pls...if something is confusing just ask pls |
1/24/2012 11:06 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, The only methode to get a DB to memorycard is using the option Program Memory Cartridge and check the Data Block box. If that DB is on the cartridge CPU will startup using the data in that block. When you (normal)download the PLC with RCP/DAT checked, only the RCP/Dat files are downloaded to cartridge. I have attached a series off printscreens to show. Regards, Marcjan Attachmentmemcard_200.pdf (158 Downloads) |
Problem solved? |
|
1/24/2012 11:47 AM | |
Posts: 31 Rating: (0) |
Fala lipa marcjan POZDRAV |
Follow us on