11/5/2016 7:06 AM | |
Joined: 9/29/2016 Last visit: 2/26/2024 Posts: 25 Rating: (3) |
I am having the same problem in cpu 226 CN . i have disabled the run mode edit to increase the memory to 24kb and when i download the program of 23 kb it shows compile error. in PLC information it shows non-fatal error 82. even using other program of 19kb it shows the same error ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/6/2016 9:13:49 PMNew subject after splitting |
|
11/5/2016 12:08 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Have you already seen this thread: S7200 non fatal error(82) - Entries - Forum - Industry Support - Siemens perhaps might help you |
Follow us on