Industry Online Support
Technical Forum
9/5/2012 10:14 AM | |
Posts: 148 Rating: (14) |
I have CPU 313C and I am using its 3 High speed counters . do I have to left the 3 DO (Q0.0, Q0.1, Q0.2 ) empty ? I have attached the counting Pin assignment table . Attachments7300_cpu31xc_counting Pin table.pdf (131 Downloads) |
9/5/2012 2:56 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665)
|
Hello Amir; The DO are totally independant of the inputs, either used as standard or high-speed DI. So you should be able to use them in your program directly. Why do you ask, have you experienced a specific problem? You seem to think that D0 is available as Q0.0; not true, look at you HWConfig information for your CPU's integrated I/O. As you can see from the attached document, D0 starts at address Q124.0, D1 is located at Q124.1… You will find information on all 31xC CPUs in the following manual: SIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/5/2012 2:59 PM |
|
Follow us on