9/23/2015 10:50 AM | |
Joined: 9/14/2011 Last visit: 4/11/2024 Posts: 19 Rating: (0) |
Hello All I am a service engineer, i attend for a compliant on OEM supplied Compressor system and uploaded the program,as one ai failed i wanted it to assign to spare AI,now my Q is I cant able to see the PIW address in the program which are physical wired and the values are updating in HMI(MP277 10" touch). Is their any other way to read the analog input without using PIW in the program. plz help me out the machine is in shutdown. i m attaching the program for u r reference. Regards PKK Attachment_CMPRSR_.zip (85 Downloads) |
Follow us on