7/14/2020 12:27 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello milatsi; If you are planning to use the PAC3200 as a powermeter and need to discuss a preference between Profibus and Profinet communications with the PLC, then it all depends on your familiarity on both of these communication networks. In both cases, establishing comms with a PAC3200 requires the purchase if an expansion pack to be installed in the unit, so you have to take the cost into consideration. Select the network you are most familiar with, study the manuals explaining how to setup the PAC3200 as a DP slave or an IO device, and plow through the installation and setup. Both networks will give you similar results. Sentron PAC expansion modules- Profibus-DP and Profinet Sentron communication blocks for Profibus-DP and PN https://support.industry.siemens.com/cs/ww/en/view/109765658 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
7/16/2020 11:29 AM | |
Joined: 7/13/2020 Last visit: 5/10/2024 Posts: 6 Rating: (0) |
Hi Duris_I, I made some extra tries but had the same results... Here are the screenshots from the application... any suggestion ?? thanks anyway... Attachment314C 2PN-DP Diris A40.docx (69 Downloads) |
7/16/2020 11:36 AM | |
Joined: 7/13/2020 Last visit: 5/10/2024 Posts: 6 Rating: (0) |
Sorry what do you mean?? It is a word document... |
7/16/2020 11:43 AM | |
Joined: 7/13/2020 Last visit: 5/10/2024 Posts: 6 Rating: (0) |
Ok i made it PDF file...
Attachment314C 2PN-DP Diris A40-converted.pdf (70 Downloads) |
7/16/2020 12:06 PM | |
Joined: 7/13/2020 Last visit: 5/10/2024 Posts: 6 Rating: (0) |
Thanks Duris_I, it worked OK...!!! Everything is fine now , thanks again best regards... |
Follow us on