10/14/2015 1:22 PM | |
Posts: 112 Rating: (0) |
Hello guys. i have installed cpu 315-2DP. It works well, but sometimes it goes to STOP mode and turn on the SF led. If i change the key from RUN mode to STOP mode and than from STOP to RUN, it works well again. I check all module and looks fine. Can you help me how can i find a solution for this case please? My HW configuration is like in a photo. Thanks Adi ------------------------------------------------------------------------------------------ |
Last edited by: mr.adi at: 10/14/2015 1:23:32 PMLast edited by: Min_Moderator at: 10/14/2015 2:53:33 PMNew subject after splitting Last edited by: mr.adi at: 10/14/2015 4:12:54 PM |
|
10/14/2015 3:19 PM | |
Posts: 112 Rating: (0) |
Ok i will send diagnostic log here. Thanks Adi AttachmentDiagnose3.txt (360 Downloads) |
Last edited by: mr.adi at: 10/14/2015 3:19:27 PM |
|
10/15/2015 8:05 AM | |
Posts: 112 Rating: (0) |
Hello IN-SERVICE So, you think that i have a problem with DP slave Adr. 4 which is Adr that I marked on HW configuration? Thanks Adi
|
10/15/2015 8:38 AM | |
Posts: 8946 Rating: (999) |
Please give us the complete HW-config with all adresses for further checking. |
10/15/2015 8:54 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
I don´t think so Have a look at the time, when the entries were written in the buffer. between this entries, you mentioned and the CPU-Stop are more than 2 months. there were problems with the DP-Slave Adr. 4 in August, but on 13th Oct. the CPU went to Stop due to an IO-Error with no further information. Maybe a firmware-update can help. You can download it here: Operating System Updates for CPU 315-2DPread the information in this entry. hope this helps, regards, |
FCK WAR! |
|
10/16/2015 8:42 AM | |
Posts: 112 Rating: (0) |
Thanks IN-Service. I appreciate your advice but please read all of my diagnostic log and than tell me why this alarm goes CPU to STOP mode after 3 months?
AttachmentDiagnose DELTA.txt (193 Downloads) |
Follow us on