3/27/2015 9:55 PM | |
Posts: 5 Rating: (0) |
Hello All, Recently we had a power surge on one of our machines that wiped out the SCADA PC. After replacing the PC we rebooted the machine and now have bus faults on some of our field components (connected via Profibus). I can see the field buses blinking/triggering while they attempt to make a connection. Not ALL of the field buses are showing this error. I uploaded the diagnostic buffer file with this post. I noticed that the "bad" components change every time i update the diagnostic. Can anyone provide some advice on where to begin troubleshooting with this. I have already checked all of the ProfiBus connections and they are secure. I suspect the PLC might have issues due to the power surge but then I would also expect all of the field buses to show communication errors which is not the case here. Thanks for your time and help! AttachmentDiag_Buffer_Mar26.txt (163 Downloads) |
Follow us on