1/21/2017 5:30 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Tolis, Can u share HW configuration? The parameters of both redundant CPUs must be identical in order to run H-redundancy. How many CPs u r using? For more availability, CPs should have different subnet name but identical IP addresses. Please refer STEP 7 - Fault-Tolerant Systems(S7hvsysb.pdf )manual [installed after Step-7 in documentation]. Also note that parameter assignment error also comes if there is wrong parameters for IO modules. Please share diagnostics buffer log. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on