5/4/2009 11:59 AM | |
Joined: 12/2/2008 Last visit: 2/2/2024 Posts: 107 Rating: (2) |
Hello J_Bell, I am sorry for the delay. I attach a pdf file to show which our final goal is. I presume this structure could be possible. Currenly,We only have configured the H Simatic Device I mean CPUs and CP but not the rest of devices(PCs).Now, before connecting PCs with a Wincc Project ,I am trying to do some test to check that CPs work ok. For test, I am using a laptop with one normal TCP/IP network card ( NO a CP1613). - I am using just one TCP/IP cable for the test.Firstly I connect to a CP and after to the another one. - Every CP has its own IP. - Ping to both CPs. They Both answer. - Using IE browser and Writting each IP. They both show its information - Using Diagnostics NCM S7. Now,Everything OK. - If a small program(Step7) is running on CPUs(S7400). Now,Everything OK. Now, After having got all test my new questions are: - Could a normal TCP/IP card plug on a PC instead of a CP1613 for a redundat system? - How many TCP/IP cards should it be plugged on a PC for a redundant system. One or Two? - Would we need S7-Redconnect to get our aim? Thanks for all AttachmentHWConfig.pdf (178 Downloads) |
Last edited by: guileser at: 5/4/2009 12:37 PMLast edited by: guileser at: 5/4/2009 12:23 PMLast edited by: guileser at: 5/4/2009 12:00 PM |
|
Follow us on