8/29/2012 9:39 PM | |
Posts: 123 Rating: (5) |
Hello, If it matters, it's a S7-312C. |
8/30/2012 8:08 AM | |
Posts: 2348 Rating: (264)
|
31xC is grounded always - you can't break connection between CPU and backside metal plate. |
8/30/2012 8:43 AM | |
Posts: 123 Rating: (5) |
Well we did. With a tape So my question remain.
|
8/30/2012 10:06 AM | |
Posts: 2348 Rating: (264)
|
Can you place wiring scheme of CPU, PS and integrated modules? |
8/30/2012 1:29 PM | |
Posts: 123 Rating: (5) |
The RC-chain is a part of the S7-300 PLC (not CPU 31xC), see attachment. Using the RC-chain may be useful in some case of ground-fault monitoring. My question is: is the R value of the RC-chain then the isulation resistance between the CPU and earth? Because the chosen CPU312C doesn't have a RC-chain, it's not suitable for the unearthed DC control installation. Our solution was to put a tape (insulation layer) between the cpu ground connection and the rack in the cabinet (earth). - The cabinet is grounded. - I have isolated power supply. - No analog modules, just digital. (But I'm also curious for the case with analog modules) I think this design is wrong because the CPU have no way to discharge static charge build-up. But we decide to keep the current situation as it's. What kind of problems could we expect then?
Attachmentplc_rc.pdf (108 Downloads) |
8/30/2012 6:27 PM | |
Posts: 123 Rating: (5) |
I still appreciate your help. Thank you |
Follow us on