6/8/2007 9:34 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, To be exact, routing via Profibus and MPI is possible. This means if WinCC flexible is connected to profibus and the panel to MPI the a transfer is possible. Also if WinCC flexible is connected to MPI and the panel to profibus. Of course the hardware (CPU) should support routing. Some time ago, some Siemens guys told me that some research about ethernet routing was started. I'm curious about the results. More information about WinCC flexible 2007 can be read on thise page. I have no idea if ethernet-MPI/Profibus-routing is supported in WCF2007. I think it is quiet a miss that WCF2007 does not support this kind of routing. |
Smurf |
|
6/11/2007 5:37 PM | |
Joined: 3/7/2006 Last visit: 4/26/2023 Posts: 42 Rating: (7) |
Thank you for answers. |
Follow us on