Industry Online Support
Technical Forum
5/5/2009 7:26 AM | |
Posts: 15 Rating: (0) |
Dear Wizard !!! AfterI have done following your manual.I have seenoutput signal in DB48.DBD18 and DB48.DBD14with high speed at 50HZ of Inverter. When at low speed I can't see any signal at DB48.DBD14 (MEAS-VAL). you could see hardware configuration that i have attachment file couldi please ask you some question? with the parameter in hardware is possible or not ?Have i adjust parameter in hardware configuration ? intergration time :100ms low speed : 0MHZ high speed : 30000000 MHZ max couting, frequency : 30KHZ could you show me to solve this problem? Attachmentcpu_313c.zip (266 Downloads) |
5/5/2009 7:31 AM | |
Posts: 15 Rating: (0) |
Attachmentcpu_313c.zip (282 Downloads) |
Follow us on