6/21/2011 5:43 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Yes, in most cases that will do the job,only if the differences of both CPU are to big that won't work (i.e. witth technolegie CPU), to be sure make a copy off your program and just try it. If not you have to do it the hard way. There are lots of threads to find about that issue. Here is a good one: /tf/WW/en/Posts/55073#top Good luck and regards, Marcjan |
Last edited by: Marcjan at: 6/21/2011 5:53 PMLast edited by: Marcjan at: 6/21/2011 5:52 PMFound a good link. Problem solved? |
|
This contribution was helpful to1 thankful Users |
6/21/2011 6:06 PM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326)
|
The new CPU is spare part compatible to the old on (http://support.automation.siemens.com/WW/view/en/41764240) |
|
|
3/27/2012 6:13 PM | |
Posts: 81 Rating: (2) |
It will work fine - unless you need to use the "additional features" of the CPU. |
7/17/2017 9:01 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7954 Rating: (162) |
New question published by Abigail is split to a separate thread with the subject CPU315-2DP Replacement ! - No changes can be made. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on