Industry Online Support
Technical Forum
1/25/2010 9:17 AM | |
Posts: 28 Rating: (1) |
Dear colleague, I has created a CPU315F project , include one F-DI and one F-DO. after compiled, there are two warning information."W: the safety program contains no reintegration for the F-I/O with the start address(LADDR) 0" Project and alarm messages in the attachment. I want to know why will this information, and How can I get rid of this information. the password is siemens thanks for your help AttachmentCPU315-F.zip (56 Downloads) |
Last edited by: oldfalg at: 1/25/2010 9:19 AM |
|
1/26/2010 2:14 AM | |
Posts: 28 Rating: (1) |
|
1/26/2010 7:32 AM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear oldfalg, if you use Distributed Safety V5.4+SP2 or higher, you should find the F_ACK_GL-block as FB 219 in the library. If you use an older version, you have to program the reintegration for every module you use in the failsafe program to avoid the warning-message. Best regards, yy1 |
Follow us on