12/7/2016 2:57 PM | |
Posts: 3 Rating: (0) |
Hi all, I have a problem connecting to an ABB as slave. I'm using the PCU318-2AJ00-0AB0 and the ABB had a DSQC 532 PROFIBUS card. I would like only to see if the ABB can communicate with the SIEMENS PLC. I have added the Diagnose as attachment. Adding a OB82 in my Blocks folder had no effect. AttachmentDiagnose1.txt (60 Downloads) |
12/8/2016 11:02 AM | |
Posts: 3 Rating: (0) |
Hi Daniel, This is my setup right now: SIEMENS 6ES7-318-2AJ00-0AB0 as master and Bosch Rexroth IndraControl L45 as slave. I have set the slave on station adres 10 with Indrawork and gave him 8 byte input and 8 byte output. In the zip file you can find the diagnostics and two pictures of the setup. Hope you can help! Thank you AttachmentDesktop.zip (45 Downloads) |
Follow us on