6/21/2012 2:14 PM | |
Posts: 137 Rating: (1) |
But i need to know what is the hardware which I'll need and what is the task for each other . Best Regards, Maher |
6/27/2012 12:41 PM | |
Posts: 137 Rating: (1) |
Ok I know how can I configure the hardware ( as a normal configuration or wrong ). so what the OBx which i am going to need ? Regards, Maher |
6/27/2012 3:57 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665)
|
Hello maher; Take some time to consult the following manual: SIMATIC Fault-tolerant Systems S7-400H You will find all pertinent information on configuring and commissioning a S7-400H in its pages. For example: Specific blocks for S7–400H ● OB 70, I/O redundancy errors ● OB 72, CPU redundancy errors SFC 90 "H_CTRL" can be used to influence fault-tolerant systems as follows: ● you can disable interfacing in the master CPU. ● you can disable updating in the master CPU. ● you can remove, resume or immediately start a test component of the cyclic self-test. NOTICE Required OBs Always download these error OBs to the S7-400H CPU: OB 70, OB 72, OB 80, OB 82, OB 83, OB 85, OB 86, OB 87, OB 88, OB 121 and OB 122. If you do not download these OBs, the fault-tolerant system goes into STOP when an error occurs. Hope this helps, |
Last edited by: dchartier at: 6/27/2012 3:58 PM |
|
This contribution was helpful to2 thankful Users |
7/2/2012 3:29 PM | |
Posts: 3 Rating: (1) |
As i know u dont need to configure OB's just create a program (CFC) and download it. It will create necessary OB's automaticly and use it... |
7/5/2012 9:28 AM | |
Posts: 947 Rating: (45) |
As I recall, absence OB70, OB72 does not cause a stop |
Last edited by: gre_m at: 7/5/2012 9:29 AM |
|
7/8/2012 10:33 AM | |
Posts: 137 Rating: (1) |
so when i make the programe what i have to do ? download it in the master cpu or in to master and standby? |
7/8/2012 6:50 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665)
|
Hello maher; This is a subject that has been discussed often on the forum, for example here: /tf/WW/en/Posts/76489 Hope this helps, Daniel Chartier |
Follow us on