12/7/2013 10:01 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello MrBin, You can select a variable of typeWORDand specify the triggerBIT of the WORD. or You can convert the discrete alarms at PLC to a WORD or UINT and transfer to a HMI. If you have more than 16 alarms you have to create a new WORD or UINT and trasfer to HMI. maybe this can help you: How can you group separate signals (variables of the "Bool" data type) to one variable of the "Word" type and again extract them from that "Word" variable (Bool - Word data type conversion)? |
Last edited by: Ste39 at: 12/9/2013 5:59 AMLast edited by: Ste39 at: 12/7/2013 10:24 AM |
|
This contribution was helpful to1 thankful Users |
7/23/2015 11:51 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
1/11/2016 12:45 AM | |
Joined: 9/1/2005 Last visit: 5/8/2024 Posts: 4099 Rating: (193) |
New question published by Microwin sp9 is split to a separate thread with the subject use of trigger bit,trigger tag,trigger address in HMI Alarms. Best regards |
My Forum is the place to personalize your profile, |
|
10/23/2017 2:51 PM | |
Joined: 6/19/2017 Last visit: 5/8/2024 Posts: 8012 Rating: (163) |
New question published by naseemk123 is split to a separate thread with the subject Can someone explain the types of data for trigger tag (int, word, uint). Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on