7/30/2016 11:21 AM | |
Joined: 12/21/2012 Last visit: 4/25/2023 Posts: 3 Rating: (0) |
Dear friends Can any one help me to create logging in .csv or excel by using wincc professional v13 when iam trying to use wincc advanced iam not able to create runtime file and trigger/event based logging in excel in different columns with one time stamp when iam using wincc professional there is no .csv logging option can any one guide with example best sri ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/1/2016 11:48:32 AMNew subject after splitting |
|
7/30/2016 11:33 AM | |
Joined: 12/21/2012 Last visit: 4/25/2023 Posts: 3 Rating: (0) |
Dear friends Is there is a possibility to create timer inside an FB ??
SRI |
8/1/2016 1:02 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello srihari.m, you can find Information about timers in STEP 7 in the STEP 7 manual: Just use the "Search" function. I can't give you a path in the manual, because the commands depend on the type of PLC you are using (300/400 or 1200/1500). Here is an FAQ that uses timers:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on