11/7/2020 11:11 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33802 Rating: (4199)
|
In the attachment a program with three possible solutions. There is certainly more. The third suggestion with I3. There I use the VM memory of the LOGO !. The counter reading is transferred to the memory via parameter VM mapping and the corresponding bits for the numbers 0-3 are then queried and assigned to the corresponding outputs.
AttachmentCircuit Diagram1 Test 0BA8.Standard.zip (277 Downloads) |
This contribution was helpful to1 thankful Users |
11/7/2020 11:18 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33802 Rating: (4199)
|
Another solution ... |
This contribution was helpful to1 thankful Users |
Follow us on