4/18/2017 11:09 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, please see page 238. https://support.industry.siemens.com/cs/ww/en/view/109744610 Continuity at boundary points When assigning parameters to a cam object, you can make three different settings in the interpolation tab. These settings specify how the runtime system should handle discontinuity at the boundaries of the cam. The appearance of the cam in SIMOTION SCOUT may be different from when it is used later in the runtime system. ● Non-cyclic: Not constant at the boundary points The runtime system uses the cam as specified, including all discontinuities at the boundaries, even if it is applied cyclically. However, the acceleration limits and moment inertia of the mechanical system / drive are the governing factors. ● Cyclic absolute: Position-continuous in the boundary points The runtime system converts the cam in such a way that is position-continuous and velocitycontinuous at the boundaries during cyclic operation, which can cause changes to occur in the characteristic. ● Cyclic relative: Constant velocity in the boundary points The runtime system calculates the cam in such a way that is has constant velocity at the boundaries during cyclic operation - within mathematical limits, which can cause changes to occur in the characteristic. or page 32: Loading a new camming A new cam is loaded by a recalling an _enableCamming command. Using the synchronizingMode parameter, the synchronization criterion is specified (e.g. at the end of the current camming with AT_THE_END_OF_CAM_CYCLE). If the transition from the old cam to the new cam is already smooth, the synchronization parameters should be selected in such a way that either the synchronization length is very small for master value reference or the dynamics are very high for the forward time reference or, alternatively, use the synchronization profile with backward time reference. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
12/21/2017 9:20 AM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (9) |
Nobody has experiences, or advices with this way of creating cams in runtime? Thanks. |