1/2/2018 1:54 PM | |
Posts: 52 Rating: (2) |
Hello, http://www.yoctoproject.org/docs/current/dev-manual/dev-manual.html#creating-your-own-layer So I added a folder "recipes-httpd" and put the apache2_2.4.29.bb file in there (found the file here: https://github.com/openembedded/meta-openembedded/tree/master/meta-webserver/recipes-httpd/apache2) And I created a kas-file as jan-k suggested here: https://support.industry.siemens.com/tf/ww/en/posts/no-bb-files-matched-when-bitbaking/181760/?page=0&pageSize=10 Now the questions: 1. Where and why do I need a "iot2000-example-image%.bbappend"-file and what do I need to write in there? 2. Do I need something else apart from the apache2_2.4.29.bb file to include the recipe? I would appreciate it if someone could help me progress in creating my own Layer. Best regards, |
1/4/2018 9:30 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
I'm attaching a tiny customization layer that hopefully demonstrates the setup clearer. It pulls in nginx, but you can probably derive your own customizations from that.Attachmentmeta-my-iot2000.zip (399 Downloads) |
This contribution was helpful to3 thankful Users |
1/4/2018 9:51 AM | |
Posts: 52 Rating: (2) |
I forgot to add the LAYERDEPENDS in my layer.conf file but now the build is running! Thank you so much for your help! |
Follow us on