2/4/2017 8:14 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hi DaytonaM, You are on the right track... Please try the following code:
As you can see, the line "On Error Resume Next" means the script is not stopped/aborted, but moves on to the next line of code during opening of Graphics Designer. When WinCC Graphics Designer is loaded, the menu is created. I don't know if there are other solutions, but I use this one and it works fine
|
Last edited by: Oreca at: 2/4/2017 8:14:50 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/5/2017 4:40 PM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Goodday Oreca, Thx! that solved my problem. The code is working fine now. |
2/6/2017 3:57 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hi there, You can just simple use the "DeleteMenu" command as the first line of code in the Sub of your custom menu generation. This will delete the menu and generate it again. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on