3/20/2012 7:01 AM | |
Posts: 165 Rating: (25) |
Dear all Attachmentmask_tags.zip (74 Downloads) |
3/20/2012 7:15 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, You can't to have more then 5 recipes in case of TP177A and without 'Recipe screens'. How to do it check in http://support.automation.siemens.com/WW/view/en/21084461 Best regards, Hristo Mihalev |
3/20/2012 7:21 AM | |
Posts: 165 Rating: (25) |
Dear UMENCHO Thanks for your reply... Then what about the tags ? Tags are masked... I could not creat at least one recipe... Thanks Regards Mothilal |
3/22/2012 11:27 AM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello, are also new added tags masked? best regards |
3/22/2012 12:09 PM | |
Posts: 165 Rating: (25) |
Hello sandman AttachmentTAGS.zip (70 Downloads) |
3/23/2012 6:56 AM | |
Posts: 165 Rating: (25) |
hi raghuk Thanks for ur reply... I am using only existing tags.. how to identify the multiplexed tags? Here I have attached my complete tag list... I have also attached the bmp format screen charts while adding the tags into the recipe... If possible please give me the sample program for creating a recipe in TP177A.. Thank you Regards Mothilal AttachmentTAGS_NEW.zip (69 Downloads) |
3/23/2012 7:35 AM | |
Posts: 65 Rating: (1) |
Hello, You just select the tag that you want to add for reciepe and go to properties. In properties See in Multiplexing. If the tag was muliplexed with other tags you cant use for reciepe. Refer the attaced pic. Just clear my doubt, where the tags(Your Reciepe Tag) have assigned. What have done with those tag in your HMI and PLC program. Regards, Raghu
AttachmentTagprperties.zip (77 Downloads) |
Last edited by: raghuk at: 3/23/2012 7:49 AMLast edited by: raghuk at: 3/23/2012 7:44 AMELLA PUGALUM IRAIVANUKKE |
|
3/23/2012 8:04 AM | |
Posts: 165 Rating: (25) |
Hello raghu No tags are multiplexed with other tags. I checked now... The tags are assigned in S7 200 CPU for time delay . Profibus communication is established between the S7 200 CPU and TP 177A. There are four setting screens in my project.In setting screens, different time valuesare set based on the recipe selection. I have attached the file... Regards Mothilal Attachmentrecipe_set.zip (80 Downloads) |
3/23/2012 8:36 AM | |
Posts: 65 Rating: (1) |
Hi, This is too different problem. If you can send your program i could analyse the problem. Regards, Raghu
|
Follow us on