8/20/2014 1:47 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
Hi, this a very bad situation. First of all you should check if all components in your system can work with the new CU320-2 and the FW V4.x. Only if this happens a chance to a CU320-2 can work. The old cf Card of CU320 is not big enough for the FW V4.x of the CU320-2 and have another bootloader which can't work with the CU320-2 so you should buy new cf card's for the CU320-2 . Or you order the old CU320 as spare part from Siemens , this control unit is available for Order as spare part until 2021. To update from CU320 to CU320-2 you should update the project data in the starter project , in the project you can update the CU320 to a CU320-2 and download it to the new CU320-2 or offline to the new CF Card of the CU320-2. If you have a project with plc which control the CU320 you must also update this project so that the plc know there is a CU320-2 and not a CU320. Regards Christoph AttachmentD:\HWList.pdf (327 Downloads) |
Last edited by: ChristophD at: 8/21/2014 6:35 AMLast edited by: ChristophD at: 8/20/2014 8:36 PMLast edited by: ChristophD at: 8/20/2014 1:51 PM |
|
8/21/2014 9:58 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
newquestion published by DavidBrownis split to a seperate thread with the subjectCU320 as spare part - what does it mean?. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on