4/30/2011 9:48 AM | |
Posts: 32 Rating: (1) |
Dear Expert, i am getting fault when going online to the device g120-cu240s-dp. It is showing- 1> power stack sw fault(F052) 2> Asic time out.(F060) 3> inverter over temperature(A0504) i have changed the cu240s dp module & replace by a new one but still the problem persists.The power gets the main supply when input power contactor is energized.When i am energizing the main i/p power contactor, then also problem persists & also in parameter r70(dc link voltage) dc voltage is showing 0 though i/p voltage of power module is 460v ac. Also in configuration tab no power module data is available...I have done the factory reset several times but always showing the same fault. Please help...i am also attaching the online screen shots. thanks, ani_1986 AttachmentPM240_power_module_fault_28042011.zip (407 Downloads) |
10/11/2022 9:11 AM | |
Joined: 8/3/2017 Last visit: 2/7/2024 Posts: 1085 Rating: (53) |
Hi, thanks for sharing your guesses! However, I'm afraid that you are 11 years late as the topic was created in 2011. Btw: no one is forced to answer here, it is also written in the forum rules. BR, Noodles |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
This contribution was helpful to1 thankful Users |
Follow us on