11/8/2013 1:03 PM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324) |
Hi, I am struggling with CX32-2 modules connected to a D445-2 When I have made offline changes and I wish to download to CX32-2 modules, then it fails consistently. See attached screenshots. The download continues until 86% (Initialisation of internal data structures) where it sits for upto 10 minutes. Eventually, it fails with an unspecified error. After this, it is impossible to reconnect to the module. Only a power cycle resurrects it due to the RAM to ROM not being performed. I have had some success with making online changes and then uploading to the PG, but sometimes, the consistency checks fail even after a "save and compile all". Is there something I should or should not be doing when using CX32-2 modules. The other devices in my project like the Sinamics_Integrated and the fiveother CU320-2's are behaving correctly. Regards, AttachmentCX32-2.zip (264 Downloads) |
11/8/2013 4:33 PM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324) |
Hey Christoph, I tried the Factory Reset, this worked ok. When I download, can I download the CX32-2 as a discreet device or do I need to re-download the hardware configuration of the D445 first. See attached, I selected only the CX32 after a factory reset and tried to download, it froze at 70% and eventuallyfailed. I will try to factory reset both CX32-2 modules and download the hardware config as well. regards, Graeme AttachmentCX32-2_Factory_Reset.zip (286 Downloads) |
11/8/2013 4:44 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, normaly you do not need a download of the HW Config when you only set the cx to factory. regards Christoph |
Follow us on