12/13/2019 7:15 PM | |
Posts: 3 Rating: (0) |
Hi! I'm using D410 DP device and cant connect to S120 integrated (I'm using profibus connection). The error is the same as other guys on this theme. I have changed adapter settings that PG/PC is the only master. But the result was the same. And also what should i do this errors like this: "Information D410 Technology package TPCAM V4.1.5.15 is not available on the controller."? What should I do? ------------------------------------------------------------------------------------------ |
Last edited by: N1kh!N at: 12/13/2019 19:19:19Last edited by: N1kh!N at: 12/13/2019 19:29:05Last edited by: Jen_Moderator at: 12/16/2019 09:14:00New subject after splitting |
|
Follow us on