9/5/2017 7:19 AM | |
Posts: 305 Rating: (2) |
D425-2 is conrtrol ,config easy ... does it has any limit ? |
9/5/2017 7:52 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
no! |
9/5/2017 9:58 AM | |
Posts: 305 Rating: (2) |
which one is control ,the same ,not limit ? |
9/5/2017 10:13 AM | |
Posts: 305 Rating: (2) |
D425-2 is control ,and 1513 is control , at config different , other is the same ? |
9/5/2017 10:23 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
direct dataexchange are not supported ! |
9/5/2017 10:56 AM | |
Posts: 305 Rating: (2) |
do you can give me any file study .... i do not how config it in IRT... |
9/5/2017 11:58 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
????? |
9/6/2017 2:57 AM | |
Posts: 305 Rating: (2) |
SIEMENS has any document guide config IRT with 1500 and SIMOTION D ( any one is controler , any one is IO-DEVICE ). at two project , or at one project ? |
9/6/2017 6:20 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
no such a document doesn't exists. |
Follow us on