9/13/2020 1:00 PM | |
Joined: 9/2/2020 Last visit: 3/5/2024 Posts: 60 Rating: (0) |
Dear all I have a problem like this but with a small difference. 1. Complete project had been loaded on the machine (with additional data) by manufacturer. 2. An expert has been uploaded that project, made some small changes and downloaded it again but without additional data. (the change is putting an axis out of run). Now i have uploaded this program. 3. The manufacturer sent me original project. . The questions are : A) What is the additional data consist of? (in the documents only source codes of programs are mentioned as additional data) B) I am going to compare these two projects, transfer source code of original program to uploaded program (i think source codes haven't been changed) and finally complete the uploaded program, then download it with additional data. is this possible? Best regards ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/14/2020 16:29:25New subject after splitting |
|
9/16/2020 7:42 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, the "additional data consist of addtional project data and sources. See chapter 7.2.6 https://support.industry.siemens.com/cs/ww/en/view/109767622 //2. An expert has been uploaded that project, made some small changes and downloaded it again but without additional data. (the change is putting an axis out of run). Now i have uploaded this program. You need the offlineproject of the expert. This is now your latest version. |
With best regards, |
|
Follow us on