9/22/2017 12:18 PM | |
Joined: 5/12/2006 Last visit: 4/13/2021 Posts: 18956 Rating:
|
Hello, open diagnostic buffer of SIMOTION and show why PLC is not go to RUN.
Christoph |
9/26/2017 12:14 PM | |
Joined: 8/25/2007 Last visit: 6/9/2020 Posts: 80 Rating:
|
Hi Christoph, I have open the Diagnostic buffer and it shows error 16#F360:BE60 as below quote: "STOP by execution system, cause: Program missing for the task Cause I am not sure what is the missing program it referred to..now i am doing a test to link D435-2DP with a DCM thru profibus. attached is the project file maybe can help to have a look? I want to Assign the DCM as an Axes so it can be used also in the Address List. Azad AttachmentSample_2.zip (6 Downloads) |
9/29/2017 9:46 AM | |
Joined: 6/19/2017 Last visit: 4/13/2021 Posts: 4593 Rating:
|
New question published by azad_dsc is split to a separate thread with the subject DCM cannot selected to be assign like a S120. Best regards |
Follow us on