Industry Online Support
Technical Forum
8/4/2011 7:47 PM | |
Joined: 10/8/2010 Last visit: 4/23/2024 Posts: 2 Rating: (0) |
I have a Simotion D445-1 that has an ET200 rack attached via Profibus. As I understand the HW Config, the I/Q address is not relevant inside the CFC code. Inside my project I have an ET200 rack in the HW Config with the following address: I addresses 1816-1817 and Q addresses 1800-1801. Also, inside the CFCcodeI have a call to "et200_nlc_pib1." How are these to values (physical address and CFC name) connected together? There must be some type of cross reference or lookup table. I have attached some pictures that show exactly what I am talking about.
AttachmentCrossReference.zip (30 Downloads) |
Follow us on