Industry Online Support
Technical Forum
6/3/2011 2:22 PM | |
Joined: 5/24/2007 Last visit: 2/14/2024 Posts: 284 Rating: (27) |
Hi Sempokryl OPC works on client computers easily using DCOM. Though it could a bit troublesome making that the DCOM services are working, it is not that big a headache. Also when you are making such connections, the DCOM connections can be done with proper user rights. You can choose sameusername or different.You would finda lot of info on internet to ste this up. one such is. the following link http://www.opcconnect.com/dcomcnfg.php Actually I am not clear on what is the application or purpose. So hope hte above helps you. Otherwise you can always come back to the forum..A lot of eager people to help you!!! Krish |
6/4/2011 10:27 PM | |
Posts: 947 Rating: (45) |
Hi Sempokryl Open pageProductSupportand find "OPC". You receive many usefull links |