2/9/2012 10:47 AM | |
Joined: 7/8/2008 Last visit: 3/26/2024 Posts: 51 Rating: (0) |
dear Mr Bermuda and darius, i do also face the similar problem. hope you can help for the solution. the problem is i have tried the siemens program on link below: https://support.automation.siemens.com/WW/llisapi.dll?aktprim=0&lang=en&referer=%2fWW%2f&func=cslib.csinfo&siteid=cseus&groupid=4000003&extranet=standard&viewreg=WW&nodeid0=16502685&objaction=csopen i also have download the sql server studio sucessfully, then set the database engine and ODBC as direct by : http://support.automation.siemens.com/WW/view/de/24677043 but when i run the winCC flex runtime, and trie d to create a data base or table , error message below arise "data source name not found, and no default driver specified" how do you think about this? am i do somethng wrong? |
Last edited by: O_Moderator at: 2/9/2012 12:35 PMnew subject after splitting from /tf/WW/en/Posts/68598#top |
|
2/9/2012 2:56 PM | |
Posts: 3037 Rating: (192)
|
Hello, Do you have configure the ODBC data source correct? You should check your settings of ODBC withthe settings in thefollowing documentation. See chapter 2.3. How do you log tags in an SQL database and read them out again with WinCC flexible? Tweety |
Follow us on