4/28/2016 5:27 PM | |
Posts: 142 Rating: (2) |
Hello all. I took data from drive monitor of CUVC drive. any one could tell me its control mode,command source?How it is receiving and transmitting data from plc and it is running on PPO4.tell me also where its 6words are using.i want to transfer this masterdrive on sinamics Attachmentemerg_ag4.35.txt (253 Downloads) |
4/28/2016 6:18 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello AttachmentCUVC_PROFIBUS.pdf (275 Downloads) |
There is no such thing as the last bug in a program |
|
4/29/2016 5:32 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
r550, r551, r552 & r553. 2 control words & 2 status words. |
4/29/2016 6:19 AM | |
Posts: 142 Rating: (2) |
thank u bro for telling me.bro please tell me how these control words bit coming from plc to drive.its coming through connector?? |
4/29/2016 6:41 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Control words - These are signals which controls the the drive. Those can be from PLC or controller. Status words - These are signals from drive to PLC or controller by which drive status is communicated to PLC or controller. In your case i.e Masterdrive VC BITS 15,14,......................0 control word 1 = KK030 Parameter value = 1.00111E+15 ---> 1001110000000000 Control word 2 = KK031 Parameter value = 1.10E+13 -----> 11011000000000 Status word 1 = KK032 Parameter value = 1.00E+14 -----> 100001000000000 Status word 2 = KK033 Parameter value = 100 ------> 100 Please refer the attached sheets & co-relate with above bit information to understand the meaning of control word & status word bit significance. Attachmentmaster drive CW_SW .pdf (287 Downloads) |
This contribution was helpful to1 thankful Users |
4/29/2016 6:57 AM | |
Posts: 142 Rating: (2) |
Thanks alot bro.i understand that connector (K0030) is control word 1 and it is getting from plc.am i ryt or wrong? |
4/29/2016 7:00 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Right. |
4/29/2016 7:02 AM | |
Posts: 142 Rating: (2) |
Thanx TechTeam but in send u told me only 5 its means 6th word not using in it?i want to know that at some places Scom2 B6500.. is connected so whats this? |
Follow us on