11/6/2019 1:53 PM | |
Joined: 11/29/2017 Last visit: 2/26/2024 Posts: 19 Rating: (0) |
Hi, I wrote a couple months ago a vbs script in WinCC Runtime V7.4 + SP1 K7.4.1.0. For logging a couple variables in a Microsoft SQL server 2014 database. The vbs does the following; Every time the program in the PLC start it will set a trigger bit that start the vbs script. It's read the current time and saves it in a internal wincc tag. If the program is done de PLC set's the trigger bit again + an extra bit so the vbs script knows it's the end of the program. Now the vbs script will read the internal tag of the start date (which is the problem!) the stop time (current time) and all the variables and write it in the database. It worked fine until now. In the attachement you will find the file and result in de database. You can see that now the start time his Month and day has switched place. Have anyone a idea why it happened now? Because in Oktober it was still fine the last good log was on 29/10/2019. Thanks in Advance. Kind regards, Ward AttachmentScript_Database.zip (43 Downloads) |
Follow us on