3/16/2010 11:22 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Grim, should be something wrong in Time Synchrinization, here a lin to explain how to do that WinCC/Options for Process Control standard configuration is: 1) PLC : set cpu properties like slave date/time 2) PLC : set comunication CP card (if used) to use time synchronization. Check correction time if you need it 3) Windows: set the right time zone and date/time in 24h format (usually dd/mm/yy hh:mm:ss) 4) WinCC: computer properties->parameter tab PLC clock setting : UTC Time basis for time display in runtime : Loal Time Zone 5) WinCC: activate time synchronization as master on System Bus using the right xnetwork card (if you have more than one) regards |
This contribution was helpful to2 thankful Users |
7/8/2019 5:34 AM | |
Joined: 4/28/2015 Last visit: 3/25/2024 Posts: 100 Rating: (4) |
same problem |
Kalleh dairy Co. |
|
Follow us on