5/4/2011 10:18 AM | |
Posts: 316 Rating: (37) |
Hi Roby, use for xx and yy an Integer Variable and it will work. Or do you have an other problem? |
5/4/2011 3:30 PM | |
Joined: 4/10/2006 Last visit: 9/11/2024 Posts: 927 Rating: (2) |
Hallo Chilly_Garfield U #init x01: U #end AUF #DBnum1 AUF #DBnum2 L #temp_1 //confronto dei due byte UN #comp_ok //se diversi resetto esito ok L #number_load //decremento indice pointer L #number_load //confronto quando ha finito di controllare UN #end x03: U #end //esito ok Attachmentvariable_declaration.pdf (84 Downloads) |
Last edited by: Roby at: 5/4/2011 3:41 PMSetting of my PG M6 Siemens |
|
5/5/2011 7:04 AM | |
Joined: 3/24/2009 Last visit: 7/9/2024 Posts: 535 Rating: (112) |
Dear Roby, the variable 'init' is placed in the TEMP-section, so it is stored in the local-data-stack. After your FB is finished, this memory-cell will be released and used by the following blocks. So the content of the variable may be overwritten. To initialise a variable in the TEMP-area, you have to write some code - it does NOT have an initial-value. Please have also a look at the excelent posting of fritz in this thread. Best regards, yy1 |
This contribution was helpful to2 thankful Users |
Follow us on