Industry Online Support
Technical Forum
8/11/2011 5:51 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello JimmyHendrix; When you say integrate, do you mean to have the possibility of sending commands and recieve status data between the DCS and the drive? Sinamics drives have a Profibus-DP port directly on the CU320-2DP controller, and can have either a Ethernet card (for Profinet-IO connection) or a CAN interface as an optional board. See the following Operating Instructions for a Sinamics S150 as an example: http://support.automation.siemens.com/WW/view/en/51829296 If these communication interfaces are not what you are looking for, what exactly do you need? Hope this helps, Daniel Chartier |
Follow us on