3/24/2020 9:29 AM | |
Posts: 32 Rating: (2) |
Hello experts, I have a problem loading my wincc project from an engineer station to a client computer configured as an engineer too, and my concern is that each time I load the proger an error message is displayed (see pj). have that someone help me to solve this problem. Best regard Attachmentpcs.docx (36 Downloads) |
3/25/2020 1:07 PM | |
Joined: 9/3/2013 Last visit: 11/3/2023 Posts: 152 Rating: (31) |
This is usually not a general issue, either the SQL server is freezed or is corruped. or your project is damaged. Regards |
3/25/2020 2:26 PM | |
Posts: 32 Rating: (2) |
Hello, But how do I fix this problem. Regrads |
3/28/2020 4:03 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Ahmed_teb, I am not quite understand the architecture still. Which one is the engineering station you showed in the document ? OSC1 or SERV13? So you are downloading from OSC1 (Engineering Station) to SERV13? And your SERV13 , you have deactivated the runtime completely and close project. So now you perform the download to SERV13, but failed with the "The SQL server cannot access data"? Can you make sure the user login account on both of the station are the same? The should have "SIMATIC HMI" authorisation. And can you also run the "Reset_WinCC.vbs" tool in C: program files \Siemens\WIncc\bin" , search it in your folder. This is to ensure all wincc application services stop and no sql is using from the background. Perform a restart and download the station again. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on