Industry Online Support
Technical Forum
7/25/2014 6:09 PM | |
Posts: 5 Rating: (0) |
All, I have a setup with 50BA7 modules all connected using ethernet. When i toggle an input from 1 logo I set an output on an other logo. When simulated everything is ok, but when i run the program on real devices i notice sometimes a delay up to 10 seconds before the output is switched. Is it because i used to much network inputs? I attached my test application. Is there someone who had this issue as well. Or, visa versa, had a comparable setup without any issues? I tried a lot of things, but now i'm out of optionsand i realy want to solve this issue. Thx
Attachmentexample.zip (147 Downloads) |
8/18/2014 5:45 PM | |
Posts: 215 Rating: (6) |
Hello, I dont think this will help. But it is possible to determine the cycle time of LOGO! Look up LOGO! manualhttp://support.automation.siemens.com/WW/view/de/50074616/0/enfor Content table "B Detrmining the cycle time" page 349. Regards |
Follow us on