12/3/2013 11:40 AM | |
Joined: 9/11/2012 Last visit: 9/14/2023 Posts: 43 Rating: (0) |
Hi Wizard, I have a need similar to the one Ruben66 described. I opened a step7 project which has a s7 project and no other intergrated project ( no Wincc flex or WinCC proj). I right clicked on the Object properties and check Required soft packages. The tool shows it needs: WinCC and WinCC flex Adv both. After that I click on "Evaluate" and then the display shows it needs WinCC only. However there is no integrated WinCC proj in this Step7 project. How can this be possible. Does it mean the WinCC proj was integrated by the programmer and then deleted at one point of time??? Thanks in advance Fredrick |