10/5/2020 1:56 PM | |
Joined: 8/22/2019 Last visit: 6/30/2021 Posts: 13 Rating: (0) |
I formatted the microSD card and wrote the Linux image provided by Siemens again. The STAT LED is blinking and doesn't stop. Now, the device is not accessible. Could you help me? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2020 08:01:18New subject after splitting |
|
10/8/2020 9:40 AM | |
Joined: 8/22/2019 Last visit: 6/30/2021 Posts: 13 Rating: (0) |
That's true. The device is not accessible anymore. |
10/8/2020 3:56 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, this state is healthy, I have no explanation for that.. You can try to connect X1P1 to a dhcp router as well as your PC. Then you need to check the IOTs IP address in the router's webserver and connect via this interface. Another thing you can do is to use a UART cable (e.g this one) to establish a serial connection and check what is going on. But honestly I think there is something going wrong with your IP addresses, if you can't even ping it in its default state. Best regards! |
Last edited by: bergmanu at: 10/08/2020 15:56:27Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on