12/21/2012 10:09 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, there are some FAQs in the internet in refer to this regards. Perhaps it could be mainful for you: http://support.automation.siemens.com/WW/view/de/63877868 http://support.automation.siemens.com/WW/view/de/43713352 With best regards |
This contribution was helpful to2 thankful Users |
1/25/2013 1:19 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello ROLLEX, For just the basic IO communication (as in your case for DI / DO) in PROFIBUS with S7-1200 you do not need additional programming blocks. DeviceStates is used to determine the I/O device operational states of an I/O subsystem. The status type can assume the following. 1: Configuration of device is active or not yet complete. 2: Device defective 3: Device disabled 4: Device exists |
Like it? Rate it! |
|
1/25/2013 3:44 PM | |
Joined: 6/13/2012 Last visit: 10/19/2022 Posts: 161 Rating: (4) |
But what is the right way to detect DO/DI profibus (and local)error's status? I know about OB82, but "multierror" is not fully do for me. p.s. what is the function of i/o system, i/o device. i/o sub.....and so on?
|
1/25/2013 4:41 PM | |||||||||||||||||||||||||||||||||
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello ROLLEX, FYI
|
||||||||||||||||||||||||||||||||
Like it? Rate it! |
|||||||||||||||||||||||||||||||||
This contribution was helpful to1 thankful Users |
1/25/2013 4:56 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello ROLLEX, 1. What do you mean by detect DI / DO PROFIBUS and local error status?? 2. OB 82 works with the diagnostics-capable modules. and again what exactly do you mean by multierror (does this mean multiple error happening at same instance of time)? |
Like it? Rate it! |
|
1/25/2013 9:22 PM | |
Joined: 7/7/2010 Last visit: 5/3/2024 Posts: 14680 Rating: (2350)
|
In the interface of OB82, one of the inputs is a bool named multierror. It means multiple errors exist meaning a smart loop must be done inside OB82 to figure out all the error reasons. I have tried figuring it out, but the documentation was lacking to figure out what to do with the multierror bit. |
science guy |
|