4/11/2017 4:44 PM | |
Posts: 1 Rating: (0) |
Buonasera, in mio possesso ho un motore mandrino codice 1PH6103-4LZ-44Z dovrei sostituirlo con un 1PH6103-4CF-44Z. Che differenza c'è tra i due motori? è possibile fare questa sostituzione? potete contattarci anche telefonicamente? ----------------------------------------------------------------------- Good evening, I have in my possession a spindle motor 1PH6103-4LZ-44Z code should I replace it with a 1PH6103-4CF-44Z. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/12/2017 2:48:49 PMTranslation Last edited by: Min_Moderator at: 4/12/2017 2:49:49 PMNew subject after splitting |
|
4/13/2017 11:01 AM | |
Joined: 10/11/2006 Last visit: 4/19/2024 Posts: 5820 Rating: (787)
|
Hello AlessandroTMB, from the article numbers I can see that there are differences in encoder type and winding version. encoder type L = hollow shaft encoder winding version Z = special winding (--> for specification options and serial number have to be checked.) Additional options have to be checked as well. Best regards TechTeam |
With best regards, |
|
Follow us on