4/1/2011 4:13 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Use the SFC1 in order to know the actual time. (How can you read out the date and time with SFC1 (READ_CLK) and input them with SFC0 (SET_CLK)? ) Devide the hours and minites from there and after make comparing with your wish time in order to energize an output which will LIGHT ON. BTW, OB10 should works with PLCSIM 5.4 SP3... Best regards, Hristo Mihalev |
4/1/2011 4:22 PM | |
Posts: 11 Rating: (0) |
ok hristo i will look on it. thanks |
4/1/2011 4:31 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
Have a look on and in this blocks. |
|
|
4/2/2011 10:15 AM | |
Posts: 11 Rating: (0) |
can we use sfc1 sgc 0 as blocks in ladder in an OB1 so as to avoid using OB10; WHICH IS THE BEST sequence using OB1 and OB10; |
4/2/2011 11:05 AM | |
Posts: 11 Rating: (0) |
HOW DO WE DIVIDE HOURS ,MINUTES; |
4/3/2011 8:43 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Use SFC0 in order to set this time. Or look there How can you set the time of an S7-300 CPU via Industrial Ethernet and via MPI? Best regards, Hristo Mihalev |
Follow us on