10/12/2018 6:26 PM | |
Posts: 1 Rating: (0) |
I realise its been a while since some activity on this thread but I need some help. I am also experiencing the same issue.Access on device config is everyone/no password but with restricted selections. I know it is not safe but this is just for test purposes now. My CPU is 1212C (6ES7 212-1BE40-0XB0) firmware V4.1. The IP is ok ( same use for program download (TIA V13 SP2)and can be pinged). I do not know what else to do after I have checked the "enable the webserver using this interface" / "activate webserver on all modules of this device". Could it be that I am usime Chrome V60 and IE V11 while on the manual it stipulates IE9/Chrome 23? I would like to presume the updates do take care of the browsers supported. Please help. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_815465 at: 10/12/2018 6:35:49 PMLast edited by: Jen_Moderator at: 10/15/2018 7:47:27 AMNew subject after splitting |
|
10/12/2018 6:47 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following FAQ might help: Why can you not access the web server of the S7-1200 CPU firmware V4.1? |
Last edited by: Jen_Moderator at: 10/15/2018 7:48:42 AMOptimized link. Eng.Mohamed Ibrahim |
|