12/25/2017 4:20 PM | |
Joined: 9/21/2012 Last visit: 9/25/2024 Posts: 4167 Rating: (464) |
You need a controller (PLC) to transmit and recieve the signals. |
12/25/2017 5:40 PM | |
Joined: 9/27/2006 Last visit: 9/25/2024 Posts: 12283 Rating: (2685) |
Hello pooya; Our friend Hati is correct in that you would expect a PLC as a mater Class 1 to control the drive or Profibus. However a Siemens HMI acts as a master class 2 on Profibus-DP, so a workaround is possible. See for example this application example explaining the steps to control a Sinamics drive with a Siemens HMI: Sinamics G/S direct connection to HMI panel You will have to adapt the command structure to your ABB drive, of course. Hope this helps, |
Last edited by: Jen_Moderator at: 12/26/2017 7:30:15 PMInserted right link. |
|
This contribution was helpful to2 thankful Users |
Follow us on