2/21/2017 7:16 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Dawei, There is a button for this available in the standard APL faceplates. See the following attachment. Lock/Unlock button, which allows to turn of messages. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/22/2017 9:44 AM | |
Joined: 11/29/2011 Last visit: 4/24/2024 Posts: 1354 Rating: (229) |
Hi, You could use the PCS 7 in Practice - Smart Alarm Hiding for that. I hope I could help |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
2/22/2017 10:02 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi dawei, It was not clear to me that you wanted to hide several blocks at the same time. One (good) option is to do the following: Go to CFC charts to the MonAnL, open the properties and unhide the parameter: MsgLock. You can interconnect the MsgLock for example to a MonDiL which is set to enable/disable messages. You can also use MonDiL to set the lock/unlock automatically based on the process conditions. See the attachment on how to do this. MsgLock will disable all messages or all messages except process control messages. You can set this at the Feature.Bit25. See the helpfile for more info about Feature. And another way is to use Smart alarm hiding, which Microman suggested, but I don't know if you can manually enable/disable the alarms with a button. |
Last edited by: Oreca at: 2/22/2017 10:05:40 AMLast edited by: Oreca at: 2/22/2017 10:25:50 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/23/2017 2:24 AM | |
Posts: 5 Rating: (0) |
Hi Oreca, Thanks for help. I will try it once I am on site. |
2/23/2017 9:18 PM | |
Joined: 11/29/2011 Last visit: 4/24/2024 Posts: 1354 Rating: (229) |
Hi, The Automatic alarm hiding is working with the "Hiding Matrix" and it is configurable offline. See the "3.2 Automatic Alarm Hiding" chapter in the PCS 7 in Practice - Smart Alarm Hiding. I hope I could help! |
- What you read here, please check with manuals and your requirements. |
|
Follow us on