9/3/2013 2:28 PM | |
Posts: 1299 Rating: (135) |
Hello, Did you enable "Start Sm@rtServer" in the runtime settings > services? For more information use this getting started: https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=54122888843&Language=en-US&TopicId=44016070539 K!ke |
9/3/2013 2:32 PM | |
Posts: 101 Rating: (6) |
No, I did not enable. And it is not enabled in any of my projects. |
9/3/2013 3:55 PM | |
Posts: 1299 Rating: (135) |
You can make a new project or use a demo project and check if the problem still exists or is only caused by your project. |
9/4/2013 11:02 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can stop the Sm@rt Server under Control panel > WinCC Runtime Advanced Internet > Remote > Button "Stop". You must disable the option " Start automatically after booting" in this settings. Tweety |
This contribution was helpful to5 thankful Users |
9/4/2013 11:19 AM | |
Posts: 101 Rating: (6) |
Thank you! This solved it. |
This contribution was helpful to1 thankful Users |
8/28/2017 2:10 PM | |
Joined: 8/21/2014 Last visit: 4/25/2024 Posts: 950 Rating: (13) |
New question published by hamza aouedj is split to a separate thread with the subject When i click to Change Settings of the sm@rtServer , the application Crashes , and i need to cancel it form Windows Task Manager.. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on